What is difference from TWR-K70F120M Rev 1 vs TWR-K70F120M Rev C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is difference from TWR-K70F120M Rev 1 vs TWR-K70F120M Rev C

490件の閲覧回数
muratdemirtaş
Contributor I

Hello friends,

I'm trying boot ucLinux to our TWR-K70F120M Rev 1 boards. I can successfully compile kernel and u-boots but. When i flashing u-boot to integrated flash, i see nand blocking errors. This errors cant seen from emcraft u-boot 1.3.2 tags release. 

Are the differences between revisions a reason for not using nand flash?. u-boot 1.3.2 version can load linux images successfully without nand flash load support. I guess after u-boot releases was designed for TWR-K70F120M Rev C. What can i do? Thanks.

So this must be different problem. 

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

431件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

From what I know, there has no much difference between the Rev A and Rev C of the TWR-K70F120M. All the difference between the Revs had been listed on the first page of the schematic.

pastedImage_1.png

All the changes are nothing to do with the NAND flash. So what you mean of the NAND flash change for U-boot?

0 件の賞賛