I am trying to get two TWR-K21F120MA boards to talk to each other over multiple different interfaces and don't know what all I need to get to do that. The Interfaces are I2C, SPI, CAN, UART, and I believe the last one is called EMI. Can some one give me an idea of what I need to buy to do this? plz help!
已解决! 转到解答。
Hi, Brent,
As you know that the CAN bus needs transceiver, if you want to connect two TWR-K21F120M via CAN bus, you have to establish two tower system, each tower system consists of TWR-K21F120, TWR-SER,primary elevator board and secondary elevator board, there is CAN connector on the TWR-SER board, you just need to two wires to connect them.
Hope it can help you
BR
Xiangjun rong
Hi, Brent,
From theory, you can have two K21 processors communicate via any interfaces:I2C, SPI, CAN, UART, but from hardware simplicity, I suggest you use SPI, UART,I2C modules, the CAN needs transceiver, if you use RS232 protocol between two boards, the UART transceiver is required.
If you use SPI modules, you can connect the follwoing signals:
master SPI Slave SPI
PCS /SS
MOSI MOSI
MISO MISO
SCLK SCLK
GND GND
If you use UART without RS232
UART of K21 UART of another K21
Tx Rx
Rx Tx
If you use I2C, connect the SCL and SDA with pull-up resistors, and connect the SCL and SDA respectively.
In SDK2.0, we provide the example between master SPI and slave SPI, I think you can refer to the example.
C:\DriverE\Freescale\SDK2.0_K64F\boards\frdmk64f\driver_examples\dspi
Hope it can help you.
BR
Xiangjun Rong
Hi, Brent,
As you know that the CAN bus needs transceiver, if you want to connect two TWR-K21F120M via CAN bus, you have to establish two tower system, each tower system consists of TWR-K21F120, TWR-SER,primary elevator board and secondary elevator board, there is CAN connector on the TWR-SER board, you just need to two wires to connect them.
Hope it can help you
BR
Xiangjun rong