TWR-K65F180M: problems accessing address 0x4003A000 on Kinetis K65 MK65FN2M0VMI18

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K65F180M: problems accessing address 0x4003A000 on Kinetis K65 MK65FN2M0VMI18

837件の閲覧回数
silentlab54
Contributor III

Hi,

I'm using the evaluation board TWR-K65F180M, which is built on the Kinetis MCU MK65FN2M0VMI18.

I'm trying to configure FlexTimer 2 but I'm experiencing a problem: when I try to access the register FTM2_SC (which is the base peripheral address: 0x4003A000) the system hangs to the DefaultISR interrupt (which is located on the file Startup_MK65F18.S).

 

I'm using KDS 3.1.0, a Segger J-Link Debugger and the Project uses the Kinetis 1.3 SDK (specifically built for the specified processor K65) with Processor Expert; I obtain the same (bad) results with a bare-metal project.

 

It looks strange that I cannot access to a well-documented memory-mapped register; the situation is strange because i can access without any problems to FlexTimer 0 and 1 (peripheral base registers: 0x40038000 and 0x40039000).

 

I have already checked the chip documentation, the evaluation board documentation and the mask errata for the chip, without finding any solution to the problem.

I have attached the a simple project to simplify the diagnose of the issue.

 

Thanks in advance for your answers.

Original Attachment has been moved to: K65F180_FTM2_problem_project_example.zip

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

631件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi silentlab54,

Sorry for my late reply!

You can try to enable the clock gate of FTM2 by using SIM_SCGC6[FTM2] instead of using SIM_SCGC3[FTM2].

The Processor Expert use SIM_SCGC3[FTM2] as default.

FTM2 ClockGate.png

I am still waiting for the reply from our Processor Expert team, and I will give you the feedback when I get it.

Best Regards,

Robin

0 件の賞賛
返信

631件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Is it possibe that the library code forgets to enable the clock to the second FlexTimer module before use, or possibly it enables it in the wrong SIM register?

Eg. FlexTimer 1 clock is enabled by bit 0x02000000 in SIM_SCGC6 but FlexTimer 2 clock is 0x01000000 in SIM_SCGC3

Regards

Mark

HW timer guide: http://www.utasker.com/docs/uTasker/uTaskerHWTimers.PDF

http://www.utasker.com/kinetis.html

0 件の賞賛
返信

631件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi silentlab54,

I got the same result when using KDS3.2 with KSDK1.3 and Processor Expert.

I have create issue to our related team, and I will give you the feedback when I get it.

Best Regards,

Robin

0 件の賞賛
返信