TWR-K60F120M - ADC -ADC1 DP0 and DM0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60F120M - ADC -ADC1 DP0 and DM0

1,536件の閲覧回数
dineshVaghela
Contributor II

i am using TWR-K60F120M . i need a code to apply Differential input to ADC1 DP0 and DM0

please let me know if anybody is having this

ラベル(1)
4 返答(返信)

779件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer attached CW V10.4 Processor Expert tool generated ADC1 differental sample code.

Wish it helps.

779件の閲覧回数
dineshVaghela
Contributor II

Thanks for your Help

For AD1_DP0 and AD1_DM0.

Both channels individually working fine  when configured as single ended input.

Problem Comes when,

I configured both the channels as differential input,

I applied 0.6V as input to both the channels,

As per the datasheet,input to the differential pins must be shifted by 0.6V.

so if on both the channels I applied 0.6V to the ADC then Readings of ADC must be 0. but the reading i got is garbage values in TWR Kit.

then i applied sine wave shifted by 0.6V on both the channels but i am getting garbage readings.

I need your help regarding this issue.

Thanks

779件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Today, I do a test with TWR-K60F120M board. I connect ADC1_DP0 an ADC1_DM0 with 0.6V voltage and I could get the ADC1_RA register value is 0xfff6 or 0xfff5. For the 16-bit differntial input, the ADC conversion result is signed 2's complement. I think my test ADC1 conversion result is good. Could you let me know what's your ADC1_RA result about connect ADC1_DP0 and ADC1_DM0 with same 0.6V voltage? Thanks.

779件の閲覧回数
dineshVaghela
Contributor II

Hi,

I am interfacing ADC0_DP0 and ADC0_DM0 as differential input.

and i am using Keil as programmer.

I have attached my code.in that

DEMO.c is main file and ADC_New.c and ADC_New.h are driver files for ADC

in my code,

i have used systick timer as 1ms interrupt.

i am taking 20 samples and displays it into UART of TOWER KIT.

both the channels as single ended working fine but as i make it differential then below 20 samples  I am getting

ffc5, 19, 14, 1a, 20, 15, 13 ,f ,12 ,14 ,16 ,a, 18 ,e, 23, 1e, 1e, 1d, 13 ,15.

kindly also provide your code with UART.

My main purpose is to measure differential SINE Wave.

Thank you so much for your valuable reply.

0 件の賞賛