Hi,
I am having some trouble using the SPI module on my FRDM-KEA128. I am trying to change voltage output on a MCP4912. I compared my SPI signals to an example on the datasheet. They seem correct to me, but I'm still not detecting any voltage change. Is there anything I am missing?
The following image is me trying to send two bytes: 0xFA and 0xAA. I tied LDAC pin to ground, so voltage should be updated when a 16bits message is received.
解決済! 解決策の投稿を見る。
The image uploaded of the oscilloscope shows the 0xFA and 0xAA, the SPI seems right, from KEA128, this can be an issue with the MPC, you need to consult the datasheet from the MCP or contact the vendor of that device. I suggest reviewing the velocity of the MCP has support.
The image uploaded of the oscilloscope shows the 0xFA and 0xAA, the SPI seems right, from KEA128, this can be an issue with the MPC, you need to consult the datasheet from the MCP or contact the vendor of that device. I suggest reviewing the velocity of the MCP has support.
Hello, there are many ways to get an internal trigger but all need setting to guarantee the time. the other way with the minimum setting is to use the SysTick_Handler, but I suggest the use of the PIT or RTC.