Recommended PAD dimensions for the 98ASA00525D (QFN 16-pin) package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommended PAD dimensions for the 98ASA00525D (QFN 16-pin) package

Jump to solution
808 Views
yasushihasegawa
Contributor III

Dear NXP team,

Our customer wants to use "MKL02Z32VFG4".
The package is "QFN 16-pin" and the document is available from the following.
    https://www.nxp.com/docs/en/package-information/98ASA00525D.pdf

The customer has started designing the board, but I would like information on the recommended pad dimensions for the board side of this package.

Best Regards,
Yasushi Hasegawa

0 Kudos
1 Solution
697 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Yasushi,

 

Please check the following document that provides assembly guidelines for QFN packages.

https://www.nxp.com/docs/en/application-note/AN1902.pdf 

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
698 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Yasushi,

 

Please check the following document that provides assembly guidelines for QFN packages.

https://www.nxp.com/docs/en/application-note/AN1902.pdf 

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

697 Views
yasushihasegawa
Contributor III

Dear Felipe-san,

Thank you for your answer.

Best Regards,

Yasushi Hasegawa

0 Kudos