Re: CodeWarrior MCU V10.3 - PE Support for MK40DX256VMC7 121MAPBGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: CodeWarrior MCU V10.3 - PE Support for MK40DX256VMC7 121MAPBGA

465件の閲覧回数
lategoodbye
Senior Contributor I

Hi,

i have nearly the same problem as ride. I want to use the MK20DX256VMC7 (MAPBGA, 121 pin) in CodeWarrior 10.3, but this variant is also unavailable in Processor Expert.

Which variant would be the closest fit?

Is there any way to add support manually for CodeWarrior?

Are there any plans to add 121-MAPBGA packages in the next MCUs Driver Suite for Processor Expert?

Thanks in advance.

0 件の賞賛
返信
2 返答(返信)

320件の閲覧回数
JimDon
Senior Contributor III

You should ask this in the Processor Expert Software forum.

Other than the picture, I don't know that the package effects the code generation.

0 件の賞賛
返信

320件の閲覧回数
lategoodbye
Senior Contributor I

Hi Jim, i started a new discussion in the PE forum. Sure the package had a great influence on code generation, because the available variants have less pins than 121.

0 件の賞賛
返信