R&D work to replace MK10DN32VFM5 with MK10DX32VFM5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

R&D work to replace MK10DN32VFM5 with MK10DX32VFM5

463 Views
JRIIS
NXP Employee
NXP Employee

So I understand that N stand for No-Flex Flash Memory and X stands for Flex Flash Memory.

The X version has a dual Flash bank (2*32kB) and can be firmware updated in the field – swapping between the 2 banks.

Could you please confirm that the first 32KB memory will be the same – so it can be used as a replacement.

Some details:

MK10DN32VFM5: Kinetis K10: 50MHz Cortex-M4 Performance MCU, 32KB Flash, 8KB SRAM, 32-QFN

MK10DX32VFM5: Kinetis K10: 50MHz Cortex-M4 Performance MCU, 64KB Flash, 8KB SRAM, 32-QFN

If  MK10DX32VFM5 is not a drop in replacement with MK10DN32VFM5 then please describe the R&D effort it take to do the replacement?

This request is comming since the avalibility on MK10DX32VFM5 is better than MK10DN32VFM5.

Thanks,

/Jakob

Labels (1)
0 Kudos
1 Reply

419 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Jakob,

There isn't any work need to be done to replace MK10DN32VFM5 with MK10DX32VFM5. They share same RM, DS and errata. They have same mask 4N86B.

Regards,

Jing

0 Kudos