Processor Expert and GPIO LDD on Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert and GPIO LDD on Kinetis

4,753件の閲覧回数
Jeinstei
Contributor II

I'm not sure if I should throw this here or in the Codewarrior forums, but lets see what people think.

 

We can't seem to find a wya to use the GPIO_LDD to set pull up or pull down for any pins. While the Init_GPIO bean can do it, are we missing some option in the GPIO_LDD that can enable pull up or pull down for specific pins?

 

Thanks.

0 件の賞賛
返信
5 返答(返信)

2,790件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

the attached pdf should help you to set the pull-up in GPIO_LDD. However in future this behaiour should be improved.

 

best regards
Vojtech Filip
Processor Expert Support Team

 

 

0 件の賞賛
返信

2,790件の閲覧回数
ETCTim
Contributor I

Could you please post the PDF again?

0 件の賞賛
返信

2,790件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If it is about using pull-ups and pins with BitIO_LDD, then this might be helpful:

Tutorial: Bits and Pins with Kinetis and the FRDM-KL25Z Board | MCU on Eclipse

Hope this helps.

0 件の賞賛
返信

2,790件の閲覧回数
ETCTim
Contributor I

Yup. Great. Thanks,

0 件の賞賛
返信

2,790件の閲覧回数
Jeinstei
Contributor II

Thanks for that. We'll work with it this way for now. Hopefully it can be integrated a bit better in the future!

0 件の賞賛
返信