In the 144 pin 100MHz K60, the FB_CLKOUT signal could be muxed out on PTC3 as ALT5. In the K60P144M150, the FB_CLKOUT doesn't appear in either the reference manual (Rev 2) or the datasheet (Rev 4). The ref manual shows PTC3-ALT5 as undefined and the datasheet shows it as CLKOUT (as in system clock out, same as PTA6-ALT5). Where is FB_CLKOUT now? Are both docs wrong?
已解决! 转到解答。
Hi Steven, as Norm mentioned, the FB_CLKOUT signal is assigned to pin 106 / / PTC3, there is a small error in the device's datasheet where the pins is shown as the system CLKOUT, you can confirm the FB signal configuration in the TWR-K60F120M schematic page 4:
http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K60F120M-SCH.pdf
Hi Steven, as Norm mentioned, the FB_CLKOUT signal is assigned to pin 106 / / PTC3, there is a small error in the device's datasheet where the pins is shown as the system CLKOUT, you can confirm the FB signal configuration in the TWR-K60F120M schematic page 4:
http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K60F120M-SCH.pdf
There has been extra functionality added to the CLK_OUT pin. It can be routed out through PTC3-ALT5. However you can now select which clock is passed out of CLK_OUT pin. It is controlled through the SIM register SOPT2. The default clock_out function is FB_CLKOUT.
I'm using the flex bus with the CLKOUT pin configured for the flexbus clock.