Pin 38 (NMI_b/EZP_CS_b) on 100pin LQFP MK22FN512VLL12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin 38 (NMI_b/EZP_CS_b) on 100pin LQFP MK22FN512VLL12

851 次查看
ashrafsarameh
Contributor I

HI,

What is it used for?

Do I pull it high/low?

0 项奖励
回复
1 回复

566 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Ashraf,

EZP_CS is the chip select for signaling the start and end of serial transfers.(For more detail about EzPort, please read "Chapter 30 EzPort" in K22P121M120SF7RM)

30.2.2 EzPort Chip Select (EZP_CS).jpg

If the NMI input is low and the NMI function is enabled in the NMI_DIS field, this results in an NMI interrupt. The processor executes an Exception Entry and reads the NMI interrupt handler address from vector-table offset 8. The CPU begins execution at the NMI interrupt handler.

If you don't need these function, external 4.7 kΩ to 10 kΩ pullup is recommended.

These two function can be disabled in the flash option register (FOPT).

Table 6-3. Flash Option Register Bit Definitions.jpg

If you want use this Pin as GPIO function, please refer below:

  Using the NMI_b pin as GPIO on KL15 device 

  Disable NMI_b pin/interrupt KL04Z?

  Need to use pin PTA4 but not as NMI_b (KL15)

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------