Hi there,
we want to use the KL02Z32 hence the small package with 32/4Kb. But the datasheet I find is not sufficient for any Hardware development.
Can someone guide me with where to start and where to find user manual of the KL02 ?
Thanks you very much
Ralph
Hello Ralph,
What about your chip full part number ?
Refer to the information you give : 32/4Kb , you can refer to this RM:
If it not the RM of your chip , please tell me the part number of your chip .
Hope it helps
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Alice
Yea, yepp, I should know better what I want.
My challenge is that I have to design the board first, before I can dive into the firmware development for out board. I am completely novice for the Freescale MCU flavors. (not to ARM so)
We are using the MKL02Z32VFG4 of the family and I have problems to figure out the pin assignment for the two wire debugger. Isn't a reset pin needed for this?
Also I need to set up one pin to wake up the MCU from deep sleep.
Any reference schematics for that chip flavor would help a lot too.
Thanks
Ralph
I did, but this is a multi pin MCU.
I am using the 16pin QFN version so many info given are not for me. I was hoping to get help in filtering what is relevant for me.
I fired up the MCU professor in the IDE and see the pins I can configure for the reset, clk and data pin.
Am I completely free to choose from the selection or there are any recommendations on that little chip ?
And what are the pin SystemControl/scb_nm for ? the manual it doesn't find that term.
thanks
Ralph
Hello Ralph,
Yes, you need refr to the Pinout Joey mentioned , then configure the register of PORTx_PCRn -> MUX :
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Normally there is only one option for reset, clk and data pins per MCU.
In the reference manual here http://cache.freescale.com/files/32bit/doc/ref_manual/KL02P32M48SF0RM.pdf
Look at section 10.3 Pinout. It will tell you which pin is used for which function.