Hi, Is HCI loopback possible with KW35/36 ? if yes, can you please share the procedure ?
Hi Mario,
Greetings for the day!
Many thanks for your instant reply, I tried sending HCI_Read_Loopback_Mode in KW36 by using the following procedure :
1) Flashed the HCI_BB in KW36.
2) Opened test tool and tried sending HCI_Read_Loopback_Mode.
I receive the return parameter as Unknown_HCI_Command_Error.
What i need to know is that, IS HCI_Read_Loopback_Mode/ HCI_Write_Loopback_Mode possible with KW36 ?
Many thanks in advance!
Regards
Sai Kalyan
Hi skalyan2@visteon.com,
These commands should not be supported, I will confirm with R&D further, and will reply to you as soon as I have the results.
I see the following explanation in the BT core spec, maybe, this does not apply to Bluetooth LE, it is just the BR/EDR command.
This command writes the value for the setting of the BR/EDR Controller’s Loopback