[MKL26]怎么设置TMP的输入捕获模式

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MKL26]怎么设置TMP的输入捕获模式

554 Views
bishihao
Contributor II

大家好,又有一个问题,我想实现 TPM0 CH1 CH2 输出电平互补的边沿对齐 PWM,且 CH1 TPM1 CH0 CH1 相连,经 TPM1 输入捕捉后,获得 PWM 的脉宽。外部PTA12和PTA13已经与PTC2相连接。

程序大约是例程,但是TMP0和1都不进中断,好像tmp0和1都没有启动啊,为什么,

////////////////////////////////////////////////////////////////////////////////

// Definitions

////////////////////////////////////////////////////////////////////////////////

#define TPM_MOD_1TO10    0x1E0

uint16_t u16PWMDuty = TPM_MOD_1TO10*2;

////////////////////////////////////////////////////////////////////////////////

// Code

////////////////////////////////////////////////////////////////////////////////

void SIM_Init(void)

{

    SIM_SOPT2 |= SIM_SOPT2_TPMSRC(1);

    SIM_SOPT2 &= ~SIM_SOPT2_PLLFLLSEL_MASK;

    SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK| SIM_SCGC5_PORTC_MASK;

    SIM_SCGC6 |= SIM_SCGC6_TPM0_MASK| SIM_SCGC6_TPM1_MASK;

}

void TPM0_Init(void)

{

    NVIC_EnableIRQ(TPM0_IRQn);

    TPM0_CNT = 0;

    TPM0_MOD = 0x12C0;

    TPM0_SC = TPM_SC_TOIE_MASK|TPM_SC_CMOD(1);

    TPM0_C1SC = TPM_CnSC_MSB_MASK| TPM_CnSC_ELSB_MASK;

    TPM0_C1V = 0x00;

    TPM0_C2SC = TPM_CnSC_MSB_MASK| TPM_CnSC_ELSA_MASK;

    TPM0_C2V = 0x00;

}

void TPM1_Init(void)

{

    NVIC_EnableIRQ(TPM1_IRQn);

    TPM1_CONF = TPM_CONF_TRGSEL(8)|TPM_CONF_CSOO_MASK|TPM_CONF_CSOT_MASK;

    TPM1_CNT = 0;

    TPM1_MOD = 0x2BC0;

    TPM1_SC = TPM_SC_TOIE_MASK|TPM_SC_CMOD(1);

    TPM1_C0SC = TPM_CnSC_ELSA_MASK;

    TPM1_C0V = 0x00;

    TPM1_C1SC = TPM_CnSC_ELSB_MASK;

    TPM1_C1V = 0x00;

}

int main (void)

{

    hardware_init();    //config pee. enable all port clock;

  

    PORTA_PCR12 = PORT_PCR_ISF_MASK |PORT_PCR_MUX(0x3);                 //config PTA12,13 as TPM1 Ch0,1

    PORTA_PCR13 = PORT_PCR_ISF_MASK |PORT_PCR_MUX(0x3);

    PORTC_PCR2 = PORT_PCR_ISF_MASK |PORT_PCR_MUX(0x4)| PORT_PCR_DSE_MASK;     

  

    SIM_Init();

    TPM0_Init();

    TPM1_Init(); 

    while(1);

}

void TPM0_IRQHandler(void)

{

    TPM0_SC |= TPM_SC_TOF_MASK;

    TPM0_C1V = (uint16_t)u16PWMDuty;

    TPM0_C2V = (uint16_t)u16PWMDuty;

}

  

void TPM1_IRQHandler(void)

{

    TPM1_SC |= TPM_SC_TOF_MASK;

    TPM1_C0SC |= TPM_CnSC_CHF_MASK;

    TPM1_C1SC |= TPM_CnSC_CHF_MASK;

    //断点查看pwmm脉宽值

}

Labels (1)
0 Kudos
1 Reply

378 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Bi shihao,

I‘d highly recommend to refer to this demo and in this demo, it has made the expecting operation available.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------