Hello,
Debugging of MKL17 projects via LPC-Link2 as C/C++ NXP MCU Application broke in mcuexpresso 11.3 (windows 10)
In the 11.1 everything worked as it should, but after the upgrade, when I try to run debug session it ends with:
Didn't find chip 'MKL17Z256xxx4' vendor 'NXP' in any part information directory
information directories:
"C:/nxp/MCUXpressoIDE_11.3.0_5222/ide/plugins/com.nxp.mcuxpresso.tools.bin.win32_11.3.0.202101111546/binaries"
chip initialization failed - Ec(04). Chip name unknown in library.
I have made all the possible checks that SDK is properly installed and even tried to reinstall it but with no luck. "MKL17Z256xxx4" is shown everywhere as in 11.1 version, in the bottom right corner in all the MCU selections lists etc..
MKL17Z256xxx4 SDK is the latest one 2.8.0
解決済! 解決策の投稿を見る。
Uninstalling all the mcuexpresso versions and installing only an 11.3 fixed the issue.