MKL17 debugging as MCU App broke in mcuexpresso 11.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL17 debugging as MCU App broke in mcuexpresso 11.3

Jump to solution
942 Views
tomula
Contributor II

Hello,

Debugging of MKL17 projects via LPC-Link2 as C/C++ NXP MCU Application broke in mcuexpresso 11.3 (windows 10)

In the 11.1 everything worked as it should, but after the upgrade, when I try to run debug session it ends with:

Didn't find chip 'MKL17Z256xxx4' vendor 'NXP' in any part information directory
information directories:
"C:/nxp/MCUXpressoIDE_11.3.0_5222/ide/plugins/com.nxp.mcuxpresso.tools.bin.win32_11.3.0.202101111546/binaries"
chip initialization failed - Ec(04). Chip name unknown in library.

I have made all the possible checks that SDK is properly installed and even tried to reinstall it but with no luck. "MKL17Z256xxx4" is shown everywhere as in 11.1 version, in the bottom right corner in all the MCU selections lists etc..

MKL17Z256xxx4 SDK is the latest one 2.8.0

1 Solution
931 Views
tomula
Contributor II

Uninstalling all the mcuexpresso versions and installing only an 11.3 fixed the issue.

View solution in original post

0 Kudos
Reply
1 Reply
932 Views
tomula
Contributor II

Uninstalling all the mcuexpresso versions and installing only an 11.3 fixed the issue.

0 Kudos
Reply