I am trying to use the fast test mechanism for the watchdog peripheral.
I have it set up to perform the LOW byte test first and then the HIGH byte test if the LOW test passes. The LOW test completes with no issues. When I do the HIGH test, for some reason the watchdog does not seem to reset. I have a while(1) after I configure the watchdog, and no matter how long I wait, it never gets unstuck.
I wanted to see if anyone else has had this issue since I can't find anyone with this issue yet.
Is there something special you have to do to test the HIGH byte? Is my test failing?
已解决! 转到解答。
Hi,
I have debugged your code . The low and high byte testing works fine.But I find an issue,that it will enter high test again after reset.
And I add BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); to the project ,so that i can print debug formation.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
I have debugged your code . The low and high byte testing works fine.But I find an issue,that it will enter high test again after reset.
And I add BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); to the project ,so that i can print debug formation.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Have you configure the WDOG_CS before testing?
Do you excute this statement?
config.testMode = kWDOG32_HighByteTest;
The sdk pack has a watch dog test about byte testing. It tests low byte and high byte.
You can refer this example code that you can download from https://mcuxpresso.nxp.com/en/select.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------