MK61FN1M0VMJ15 EXTAL32 unused pin question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK61FN1M0VMJ15 EXTAL32 unused pin question

615件の閲覧回数
isaotakashima
Contributor IV

Our customer made prototype board using the MK61FN1M0VMJ15.
Previously they will use the 32.768 KHz crystal, but they decide to remove it crystal to reduce BOM cost, because they don't needed the RTC now.
According to the following discussion, NXP recommended EXTAL32 tied to GND.
https://community.nxp.com/docs/DOC-100165

However their board does not have a pattern for EXTAL32 tied to GND.

Here is their questions.
1. What kind of problem occurs if they don't EXTAL32 tied to GND even if they don't use the RTC?

2. Please let us know a reason why they should EXTAL32 tied to GND by remake the board.

Please reply immediately, because it is necessary to decide whether they remake the board by tomorrow..

Best regards,
Takashima

ラベル(1)
0 件の賞賛
返信
1 返信

421件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

That document seems haven't be updated for a long time.
The customer can refer the "Table 57. Recommended connection for unused analog interfaces" in K65P169M180SF5V2.  This document is newly updated although it is for K65.

XTAL32 EXTAL32 K65.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信