if I try to use the SPI0 of a MK20DX256 with disabled TX and RK FIFO it doesn't work.
I tried nearly everthing. I use the Config-Tool of Prozessor Expert (only the Init-Module) to set the Init-Parameter.
But regardless what I do I got only the frame below.
I init the device (see code below) and write 0xAA the TX_DATA in PUSHR. As you can see it is transmitted but the CS is only a peak
and after this transmission I can do what I want, nothing happens anymore :-( I got no more frames until doing a reset.
Have anyone an idea?
#define STOP_TRANSFER(x) (SPI0_MCR |= SPI_MCR_HALT_MASK);
#define START_TRANSFER (SPI0_MCR |= SPI_MCR_HALT_MASK);
#define SET_CONT_SCKE(x) (SPI0_MCR |= (((uint32)(x & 0x01) << SPI_MCR_CONT_SCKE_SHIFT) & SPI_MCR_CONT_SCKE_MASK))
//Clear the TX FIFO counter
#define CLR_RXF (SPI0_MCR |= SPI_MCR_CONT_SCKE_MASK)
// Clear Transfer Counter
#define CLR_CTCNT (SPI0_PUSHR |= SPI_PUSHR_CTCNT_MASK)
#define SET_CS_CONT(x) (SPI0_PUSHR = SPI0_PUSHR |(((x & 0x01) << SPI_PUSHR_CONT_SHIFT) & SPI_PUSHR_CONT_MASK))
#define SET_PUSHR(command,data) (SPI0_PUSHR = (uint32)command + data)
#define SET_TX_DATA(data) (SPI0_PUSHR = (SPI0_PUSHR & 0xFFFF0000) + data)
#define GET_RX_DATA ((uint8)SPI0_RXFR0)
// Transfer complete? 0 Transfer not complete / 1 Transfer complete
#define GET_TCF ((uint8)((SPI0_SR & SPI_SR_TCF_MASK) >> SPI_SR_TCF_SHIFT))
#define CLR_TCF (SPI0_SR &= ~SPI_SR_TCF_MASK)
// Receive complete? 0 RX FIFO is empty / 1 RX FIFO is not empty
#define GET_RFDF ((uint8)((SPI0_SR & SPI_SR_RFDF_MASK) >> SPI_SR_RFDF_SHIFT))
// this function I call in main()
void Write_Test_Byte(void)
{
// SET_CS_CONT(1); //
// CLR_CTCNT;
// CLR_RXF;
SPI0_PUSHR = (SPI0_PUSHR & 0xFFFF0000) + 0xAA; // send byte
// }
// else return(TRANSMISSION_IS_RUNNING);
for(uint32 j=0; j < 10000; j++)
{
NOP; // wait a while
}
// here breakpoint
// CLR_CTCNT;
// CLR_TCF;
}
/*
** ===================================================================
** Method : SPI0_Init (component Init_SPI)
** Description :
** This method initializes registers of the SPI module
** according to the Peripheral Initialization settings.
** Call this method in user code to initialize the module. By
** default, the method is called by PE automatically; see "Call
** Init method" property of the component for more details.
** Parameters : None
** Returns : Nothing
** ===================================================================
*/
void SPI0_Init(void)
{
/* SIM_SCGC6: SPI0=1 */
SIM_SCGC6 |= SIM_SCGC6_SPI0_MASK;
/* SPI0_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
SPI0_MCR = SPI_MCR_DCONF(0x00) |
SPI_MCR_PCSIS(0x00) |
SPI_MCR_SMPL_PT(0x00) |
SPI_MCR_HALT_MASK;
/* SPI0_MCR: MSTR=1,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=1,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=1,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=2,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
SPI0_MCR = SPI_MCR_MSTR_MASK |
SPI_MCR_DCONF(0x00) |
SPI_MCR_MTFE_MASK |
SPI_MCR_PCSIS(0x01) |
SPI_MCR_DIS_TXF_MASK |
SPI_MCR_DIS_RXF_MASK |
SPI_MCR_CLR_TXF_MASK |
SPI_MCR_CLR_RXF_MASK |
SPI_MCR_SMPL_PT(0x02) |
SPI_MCR_HALT_MASK;
/* SPI0_TCR: SPI_TCNT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
SPI0_TCR = SPI_TCR_SPI_TCNT(0x00);
/* SPI0_CTAR0: DBR=0,FMSZ=7,CPOL=1,CPHA=0,LSBFE=0,PCSSCK=3,PASC=3,PDT=3,PBR=1,CSSCK=5,ASC=5,DT=5,BR=7 */
SPI0_CTAR0 = SPI_CTAR_FMSZ(0x07) |
SPI_CTAR_CPOL_MASK |
SPI_CTAR_PCSSCK(0x03) |
SPI_CTAR_PASC(0x03) |
SPI_CTAR_PDT(0x03) |
SPI_CTAR_PBR(0x01) |
SPI_CTAR_CSSCK(0x05) |
SPI_CTAR_ASC(0x05) |
SPI_CTAR_DT(0x05) |
SPI_CTAR_BR(0x07);
/* SPI0_CTAR1: DBR=0,FMSZ=3,CPOL=1,CPHA=0,LSBFE=0,PCSSCK=0,PASC=0,PDT=0,PBR=0,CSSCK=0,ASC=0,DT=0,BR=0 */
SPI0_CTAR1 = SPI_CTAR_FMSZ(0x03) |
SPI_CTAR_CPOL_MASK |
SPI_CTAR_PCSSCK(0x00) |
SPI_CTAR_PASC(0x00) |
SPI_CTAR_PDT(0x00) |
SPI_CTAR_PBR(0x00) |
SPI_CTAR_CSSCK(0x00) |
SPI_CTAR_ASC(0x00) |
SPI_CTAR_DT(0x00) |
SPI_CTAR_BR(0x00);
/* SPI0_SR: TCF=1,TXRXS=0,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=0,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */
SPI0_SR = SPI_SR_TCF_MASK |
SPI_SR_EOQF_MASK |
SPI_SR_TFUF_MASK |
SPI_SR_TFFF_MASK |
SPI_SR_RFOF_MASK |
SPI_SR_RFDF_MASK |
SPI_SR_TXCTR(0x00) |
SPI_SR_TXNXTPTR(0x00) |
SPI_SR_RXCTR(0x00) |
SPI_SR_POPNXTPTR(0x00);
/* SPI0_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=0,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
SPI0_RSER = 0x00U;
/* SPI0_MCR: HALT=0 */
SPI0_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);
}
Yes this works... but leaded to the next problem.
After a reset and the Hardware Init-Routine of SPI0 the TCF is always 0. I have to send a dummy frame to clear it.
Futhermore I got with this code only to frames. If I have a breakpoint between the commands and execute it step by step
each command send a frame (3 frames). Without breakpoints I got only two frames. Isn't the device already ready when the TCF
is set? Never I had such probems with a SPI device :-(
#define GET_TCF | (SPI0_SR & SPI_SR_TCF_MASK) |
SPI0_PUSHR = 0x000100FF; | |
while(!GET_TCF); | |
SPI0_PUSHR = 0x000100FF; | |
while(!GET_TCF); | |
SPI0_PUSHR = 0x000100FF; | |
while(!GET_TCF); | |
NOP; |
(no command is sent befor this code)
Hi Marcus,
Do you get the same number of frames if you remove the "while(!GET_TCF);" lines from your code? Also, are you still using your original register settings or have you changed them?
Thank you,
Martyn