Kinetis Protocol Analyzer & USB-KW019032 adapter not found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Protocol Analyzer & USB-KW019032 adapter not found

1,321件の閲覧回数
ikivela
Contributor I

Hi

I just bought USB-KW019032 and tried to follow the steps in "Getting started guide"

I installed the drivers and see mbed Serial Port when dongle is connected

ikivela_0-1631685434941.png

However, when I launch Kinetis Procotol Analyzer, I don't see adapter detected.

ikivela_1-1631685526065.png

I am using Windows 10. Protocol Analyzer version is 2.0.4.1

What am I doing wrong? 

0 件の賞賛
返信
6 返答(返信)

1,281件の閲覧回数
ikivela
Contributor I

The problem persist. I can't run KPAA (version 2.0.2.1) it complains that I don't have Wireshark installed (3.2.0) eventhough I have it

 

ikivela_0-1632306395462.png

 

0 件の賞賛
返信

1,273件の閲覧回数
nxf56274
NXP Employee
NXP Employee

1 Did you close the firewall?

2 Did you put the software in 'c:/nxp'?

0 件の賞賛
返信

1,266件の閲覧回数
ikivela
Contributor I

Yes, I did that. 

I also tried Test Tool 12.6.3 but it did not either detect the device.

 

0 件の賞賛
返信

1,225件の閲覧回数
nxf56274
NXP Employee
NXP Employee

The Kinetis Protocol Analyzer doesn't support USB-KW019032. kw01 works on 1Ghz. The Kinetis Protocol Analyzer works on 2.4Ghz. So the only way is to use the test tool including the protocol analyzer. 

So you have followed the guide and use test tool to open the protocol analyzer?

nxf56274_0-1632448763601.png

 

0 件の賞賛
返信

1,308件の閲覧回数
ikivela
Contributor I

I download older version of KPAA  2.0.2.1 and Wireshark 3.2.16, but now I can't start KPAA because of error:

"Wireshark is not detected on your PC"

0 件の賞賛
返信

1,316件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer this link.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信