I use keil5, I do clock init .reference: "KL26P121M48SF4RM" of page on 416~418 24.5.3.1 Example 1: Moving from FEI to PEE mode: External Crystal =4 MHz, MCGOUTCLK frequency = 48 MHz
it running is ok ,but when I do debug,it is failed . it stopping " while((MCG->S & IREFST ) == 0x10U);" I need you help. thanks
external reference clock is 8Mhz
my code as follow
#include "MKL26Z4.h"
#include "clock.h"
#define OSCINIT0 0x02
#define IREFST 0x10
#define CLKST 0x0c
#define PLLST 0x20
#define LOCK0 0x40
void Clock_Init(void)
{
// SIM->SCGC5 |= SIM_SCGC5_PORTA_MASK;
//CLOCK_SETUP=1;
SIM->COPC = (uint32_t)0x00u;
SIM->SCGC5 |= (uint32_t)0x0200UL; /* Enable clock gate for ports to enable pin routing */
SIM->CLKDIV1 = (uint32_t)0x00010000UL; /* Update system prescalers */
PORTA->PCR[18] &= (uint32_t)~0x01000700UL;
PORTA->PCR[19] &= (uint32_t)~0x01000700UL;
OSC0->CR = (uint8_t)0x80U;
MCG->C2=0x1c; //
MCG->C1=0x98; // MCGLOUTCLK
while((MCG->S & OSCINIT0 ) == 0x00U); //
while((MCG->S & IREFST ) == 0x10U); /
while((MCG->S & CLKST ) != 0x08U); //
MCG->C5=0x03;
MCG->C6=0x40; //
MCG->C2=0x1c;
while((MCG->S & PLLST ) == 0x00U);
while((MCG->S & LOCK0 ) == 0x00U);
MCG->C1=0x18;
while((MCG->S & CLKST ) != 0x0cU);
}
Best regards,
已解决! 转到解答。
Hi,
I tested the same on a FRDM-KL26Z and CodeWarrior and found the same behavior. I saw that the behavior is related with the wrong configuration of the MCG_C2 register. In your code you are configuring:
MCG_C2 = 0x1C which is:
RANGE0 = 01 Encoding 1 — High frequency range selected for the crystal oscillator .
EREFS0 = 1 Oscillator requested.
HGO0 = 1 Configure crystal oscillator for high-gain operation.
According to the DataSheet when RANGE0 = 01 the Oscillator must have a value of Min. 3 MHz and Max. 8 MHz. Since I am using the FRDM-KL26Z with an 8 MHz Oscillator I configured:
MCG_C2 = 0x24 which is:
RANGE0 = 1x Very high frequency range selected for the crystal oscillator
EREFS0 = 1 Oscillator requested.
HGO0 = 0 Configure crystal oscillator for low-power operation.
Please check that the MCG_C2 value is configured correctly according to the Oscillator values in your hardware.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I tested the same on a FRDM-KL26Z and CodeWarrior and found the same behavior. I saw that the behavior is related with the wrong configuration of the MCG_C2 register. In your code you are configuring:
MCG_C2 = 0x1C which is:
RANGE0 = 01 Encoding 1 — High frequency range selected for the crystal oscillator .
EREFS0 = 1 Oscillator requested.
HGO0 = 1 Configure crystal oscillator for high-gain operation.
According to the DataSheet when RANGE0 = 01 the Oscillator must have a value of Min. 3 MHz and Max. 8 MHz. Since I am using the FRDM-KL26Z with an 8 MHz Oscillator I configured:
MCG_C2 = 0x24 which is:
RANGE0 = 1x Very high frequency range selected for the crystal oscillator
EREFS0 = 1 Oscillator requested.
HGO0 = 0 Configure crystal oscillator for low-power operation.
Please check that the MCG_C2 value is configured correctly according to the Oscillator values in your hardware.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
The different HGO modes can be used according to your hardware and project requirements. Please refer to the specific reference manual in the section High-Frequency, High-Gain Mode and section High-Frequency, Low-Power Mode to have a better understanding of each mode. As you can see in the Datasheet in the section Oscillation frequency specifications the HGO modes will impact directly in the Crystal startup time.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------