KL25Z board problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL25Z board problem

417 次查看
sarthakkelapure
Contributor I

I have a Freedom board KL25Z. I tried to upload my .bin file in the drive that was created but instead the board got disconnected everytime, so i tried to run it in bootloader mode and upload the MSD file from the NXP site and now the debug mode wont start, in the bootloader mode the status LED blinks for 7-8 times quickly and this goes on instead of the 1s gap, no firmware worked. Please help.

PS: I m working on Windows 10

0 项奖励
1 回复

294 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please try the method descripted in "Bricking and Recovering OpenSDA Boards in Windows 8 and 10".

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 项奖励