HI there,
I have been working with KEA8 (TSSOP 16 pins) + CW11 + MultiLink FX.
After debbug I decided to use
SIM_SOPT =0x00000000;
In order to use alternate PTA4 and PAT0 functions. Now I want to erase some devices but I cannot do it.
Using flash to file option and then erase whole device, using KEAZN8M4.xml flash configuration.
Following errors appears
Error executing task KEAZN8M4. Wrong expression ${ProjDirPath}/Project_Settings/Debugger/init_kinetis.tcl; Could not expand variable ProjDirPath
If I use debug option there is no change to connect to device, is there any workaround?
Best regards,
Marc
Hi
Sorry, not.
You can try to put the reset pin to low in order to try to start to debug it, I do not remember if the Multilink FX can provide the power to the board, I believe with this option will be easier. But I only use the Jlink
Regards