Need Sample Code to transmit and Receive CAN messages using KEA128 Micro Controller. IDE used is KEIL.
Hi Sharad Mehta,
We still don't have the keil MSCAN project for KEA128, but we have a lot of CAN drivers, and some other IDE project, take an example CW MSCAN project.
You can find the KEA128 MSCAN driver from this link::
MSCAN driver for Kinetis EA devices
The above link already contains the CW KEA128 MSCAN project, you can test it on our TRK-KEA128 board.
But if you still want to use the keil project, I think you can create a keil project, then add the above CAN driver to your keil project, then test it.
Beside the above MSCAN driver, in the attachment, I also attach another CAN CW project, it also has the CAN driver, just different format, it also works.
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi , I want to use the sample code "Can_test_nonemask250k.rar" , What version of CodeWarrior should I download, thanks.