KDS with MKE02Z64VLC4 POR and LVD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS with MKE02Z64VLC4 POR and LVD

468 Views
blsousan
Contributor III

I am needing to check/set the configuration for the POR voltage level and the LVD levels.  I see nn the Component Inspector where the LVD values can be set.  However, it shows the LVD voltage threshold can be set to  either Low or High.  (I assume the word "treshold" in the KDS tools really means "Threshold"?).  However, where can I find the exact voltage values for the settings of High and Low?   Also, is there an entry somewhere in the tools for setting the Vpor value as well?

Thanks,

Bill

0 Kudos
Reply
1 Reply

371 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Bill,

You can check this information in the datasheet:

http://cache.nxp.com/files/microcontrollers/doc/data_sheet/MKE02P64M40SF0.pdf

There is the Table 4 about LVD and POR levels. VPOR voltage is not configurable:

pastedImage_1.png

Best regards,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply