KDS/MCUXpresso IDE Support for L Series - MKL17Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS/MCUXpresso IDE Support for L Series - MKL17Z

485 Views
vikas_katariya
Contributor I

I am looking at a couple of tool-chains for MKL17Z64VFM4 - L Series, Is this supported in Kinetis Design Studio Or MCUXpresso IDE?

 

If yes, Is there a sample project which I can refer to?

0 Kudos
2 Replies

400 Views
vikas_katariya
Contributor I

I think this could help

Welcome | MCUXpresso SDK Builder 

0 Kudos

400 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Vikas Katariya,

I recommend you to use MCUXpresso IDE since is our newest IDE. 

You can download the SDK for the MKL17Z, here you will find multiple examples for the MCU.  

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------   

0 Kudos