Hi everyone,
i'm developing an OTA updater using Flash Swap feature. I successfully implemented flash swap but when i encounter an error in downloaded firmware (i use CRC to test integrity of the file) i abort the flashing and my flash remain in UPDATE_ERASED state so when i reset and retry to flash i obtain FTFx_ERR_ACCERR.
I tried to perform a flash eraser before reset after a CRC error but i don't find any examples on how return in READY state (or another reliable state) to restart flashing from initial point.
Now i perform an erase of swap indicator sector in that way:
ret = FlashEraseSector(&flashSSDConfig, PSWAP_INDICATOR_ADDR + (P_FLASH_SIZE/2), P_SECTOR_SIZE, g_FlashLaunchCommand);
if(ret != FTFx_OK)
{
return ret;
}
ret = PFlashSwapCtl(&flashSSDConfig, PSWAP_INDICATOR_ADDR, FTFx_SWAP_SET_INDICATOR_ADDR, ¤tSwapMode, ¤tSwapBlock, &nextSwapBlock, g_FlashLaunchCommand);
if ((FTFx_OK != ret))
{
return ret;
}
I erase the swap indicator in upper flash section and then set swap indicators in active flash section.
Is it correct?
已解决! 转到解答。
Hello Francesco Salvatore,
I think you are facing a similar issue as the one discussed in the next thread:
MK22FN1M0VLQ12 SWAP: Return from UpErs to Ready
The SWAP system uses a sequential state machine, not intended to move backwards (e.g. from UPDATE-ERASED to READY state).
You can stay in UPDATE-ERASED state, erase the corrupted firmware and start flashing again the correct firmware.
Please let me know if I misunderstood your situation or use-case.
Best Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Francesco Salvatore,
I think you are facing a similar issue as the one discussed in the next thread:
MK22FN1M0VLQ12 SWAP: Return from UpErs to Ready
The SWAP system uses a sequential state machine, not intended to move backwards (e.g. from UPDATE-ERASED to READY state).
You can stay in UPDATE-ERASED state, erase the corrupted firmware and start flashing again the correct firmware.
Please let me know if I misunderstood your situation or use-case.
Best Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------