K20 Can bus can not work, other functions are normal,why?
Hi
Can you detail your questions, including your hardware, and software , or debug console?
Regards
Daniel
Hello, I use my own painting PCB,The program is downloaded from the Internet.Now the situation is that the 485 communication can work, but the CAN bus to send and receive are not, with keil software debugging results as shown in Figure
Hi
I think we need to check it is a hardware issue or software issue first.
From your picture , I saw two results, one is correct , the other is wrong. what is the difference, they run in the same board?
There are two can modules in this chip, both of them can't work or only one?
If you only enable SIM , then check the register, what is the result.
Regards
Daniel
No, that part of the above is correct, that part of the following is wrong, two are not the same, now it seems to be the problem of the clock