Invalid SWDIO in Keil MDK with CMSIS-DAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Invalid SWDIO in Keil MDK with CMSIS-DAP

877件の閲覧回数
kai_liu
Senior Contributor I

Invalid_SWDIO.PNG.png

I love to use on board debugger of FRDM to debug off-board microcontroller. Today I found an issue of WRONG SWDIO.

I used to MDK since it can be used to read chip IDCODE in debugger configuration Window. The target is M0+, MKL25Z. I have multiple boards. Some boards can be read as regular as:

SWDIO: 0x0BC11477 for MKL25Z128 (M0+)

SWDIO:0x2BA01477 for MK20DX128 (M4)

0BC11477->00001011110000010001010001110111

Some other boards will be read as:

FC0E001B->11111100000011100000000000011011

05E08A3B->00000101111000001000101000111011

Due to wrong IDCODE, MDK refuses to download.

I guess it is hardware related issue. Is there anything I can do? Shorter cable? Layout issue?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

654件の閲覧回数
kai_liu
Senior Contributor I

God only helps peple who helps himself.

I guess I got it.

The target board is powered by USB. It must have small Magnetic beads on both 5V and GND. Due to PCB layout issue, I use 0R to replace them. As a result, the noise from PC comes through whole ground and power supply, I believe noise in ground is more important.

Now I add a choke coil (TDK from SONY DC) on USB cable. It works on every tested board, although I haven't test all.

Here comes new question.

Before adding choke coil, some boards always failed with wrong IDCODE. After adding, then every tested board works. Even I removed the choke, they still work.

I bought a MKL25Z board from the market, which has dedicated SWD port. The debugger always reads out wrong IDCODE from SWD port. Now I connect debugger to dedicated port, it works fine. Switching back to SWD, it works again.

So maybe it is not 100% noise issue, improper connection could be another one. If I adjust the jumper wires, sometimes it works.

However, it implicts that the device should be reviewed by a prefessional hardware engineer. I am a software engineer who is trying to make own board. :smileyplain: