I'm having problems working with UART5 to communicate with the pc through USB. I'm trying to send a message to the pc, therefore i'm only using Tx. The problem is that i'm trying to write in some registers but the values don't change. Also, i don't know how to set the baud rate to 9600 bps.
I would appreciate some help. The program is what follows:
#include "derivative.h" /* include peripheral declarations */
int main(void)
{
int i;
uint8_t message[] = "Hello World";
//enable clock to port E
SIM_SCGC5 |= 1<<13;
//enable clock to UART5 module
SIM_SCGC1 |= 1<<11;
//set pin 8 from port E as UART5_Tx
PORTE_PCR8 |= 0x00000300;
//Disable Receiver and Transmitter to change UART settings
UART5_C2 &= ~0x0c;
// Configure the UART for 8-bit mode, no parity
UART5_C1 = 0;
//Set the baud rate - > I don't know how to set the baud rate to 9600 bps
UART5_BDL = 4; //UART_BDL_SBR(9600);
UART5_BDH = 4;
//Enable Transmitter
UART5_C2 |= 1<<3;
//Writing in the transmitter data register
for (i = 0; message[i] != '\0'; i++) {
UART5_D = message[i]; - > the register doesn't change and i don't know why
}
return 0;
}
Thanks!
已解决! 转到解答。
Hi,
You will find useful the document KQRUG in the section UART initialization example you can find useful information about the UART initialization process and registers. Please refer to the document for more details.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ricardo
1. The Baud rate of UART5 depends on your Bus Clock. If you have 50MHz then 9600 Baud is obtained by
ucFraction = (unsigned char)((float)((((float)BUS_CLOCK/(float)16/(float)9600) - (int)(BUS_CLOCK/16/9600)) * 32)); // calculate fraction
usDivider = (BUS_CLOCK/16/9600);
UART5_C4 = ucFraction; // 0x10
UART5_BDH = (unsigned char)(usDivider >> 8); 0x01; // (0x145 >> 8)
UART5_BDL = (unsigned char)(usDivider); // (0x145 & 0xff)
2. UART5_D is a write register for sending data and read for receiving data. Therefore you can't read the value back that you write (send) unless the TXD line is connected to the RXD line and your receiver is also enabled.
3. You also need to modify your transmission loop since this will overrun the output - it needs to check that there is space in its output buffer/FIFO and wait if there isn't.
Regards
Mark
Kinetis: µTasker Kinetis support
K60: µTasker Kinetis TWR-K60N512 support / µTasker Kinetis TWR-K60D100M support / µTasker Kinetis TWR-K60F120M support
UARTs/PUARTs: http://www.utasker.com/docs/uTasker/uTaskerUART.PDF
For the complete "out-of-the-box" Kinetis experience and faster time to market
Hi,
You will find useful the document KQRUG in the section UART initialization example you can find useful information about the UART initialization process and registers. Please refer to the document for more details.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------