Hi all,
I am trying to setting up the envoirement to work with Kinetis design studio, what I do is:
- Install Kinetis design studio (in windows8)
- Install SDK (in windows8)
- Install SDK in Kinetis design studio (Install new software, searching the KSDK_1.0.0_KL43Z_1.0.2_Eclipse_Update.zip file...), as indicated in KDS user guide
The problem I have, is that every time I import an example (only tried usb examples), the linked resources does not point correctly and I have to change them manually. The adater file alo seems not to be well pointed because I chose bare metal and it was building like an OS was selected.
So, probably I am doing something wrong but I cannot guess what.
Anyone can help me? Does any guide or similar for using SDK examples in KDS?
I look forward your help.
解決済! 解決策の投稿を見る。
Sorry Alice for my bad english :smileysad:
I want to build virtual com bare metal project.
Once in a blank workspace:
- Import driver library and build, it works.
- Import usbd_sdk_frdmkl43z48m_bm, as you told me :smileyhappy:, and build, it works
- Import the dev_cdc_virtual_com_frdmkl43z48m_bm, it builds
I can plug the board to the PC and communicate with no problem. So it seems to work perfectly.
But when I want to write my own code inside I realize that it is not working in bare metal, OS_ADAPTER_SDK is selected, and if I change the adapter_cfg.h file to bare metal it stops working.
If I should put pictures of any message or something please tell me.
Regards,
Miguel
Hi Miguel.
Have you build the driver library ? Please refer to
"...\KSDK_1.0.0-KL43Z\doc" -> "Kinetis SDK User's Guide for the FRDM-Kl43z" -> 4.4 Kinetis Design Studio IDE .
Hope it helps
Alice
Hi Alice,
Thanks for your prompt response.
First I import the driver library, and I can build it with no errors.
If I import a demo from the demos folder I can build them, just six warnings (because search for 6 files that not exist?)
The problem is that if I import a project from C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\usb\example\device, I get this
I hope you can help me.
Regards,
Miguel
Hi Miguel,
About the USB demo , after the above operations, it need build the "usbh_sdk_frdmk43z48m_bm" lib .
it is here (...\KSDK_1.0.0-KL43Z\usb\usb_core\device\build\kds ).
Hope it helps
Alice
Hello Alice,
Yeah!! That was it.
Now it builds, and I can debug. But...
I do not know why it does not work as I expected.
It is supposed to be a bare metal project, but adapter_cfg.h file looks like this:
/**HEADER********************************************************************
*
* Copyright (c) 2013 Freescale Semiconductor;
* All Rights Reserved
*
*
***************************************************************************
*
* THIS SOFTWARE IS PROVIDED BY FREESCALE "AS IS" AND ANY EXPRESSED OR
* IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
* OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
* IN NO EVENT SHALL FREESCALE OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
* INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
* HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
* STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
* IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
* THE POSSIBILITY OF SUCH DAMAGE.
*
**************************************************************************
*
* $FileName: osadapter_cfg.h$
* $Version :
* $Date :
*
* Comments:
*
* @brief The file contains OS adapter configuration inf.
*
*****************************************************************************/
#ifndef _OSADAPTER_CFG_H
#define _OSADAPTER_CFG_H 1
#define OS_ADAPTER_MQX 1
#define OS_ADAPTER_BM 2
#define OS_ADAPTER_SDK 3
#define OS_ADAPTER_UCOSIII 4
/*#define OS_ADAPTER_ACTIVE_OS OS_ADAPTER_UCOSIII*/
#define OS_ADAPTER_ACTIVE_OS OS_ADAPTER_SDK
#endif
So, OS_ADPTER_SDK is selected, and if I change to
#define OS_ADAPTER_ACTIVE_OS OS_ADAPTER_SDK
it stops working, because compiler does not find adapter_bm.h
I do not guess why I get working OS_adapter_sdk when all the open projects are bare metal :smileyconfused:
Any sugestion?
Hi Migue,
Sorry for i'm not very clear your meaning . Could you tell me which example you want to run , and how should I do to recurrence your error step by step ?
And do you want to run the demo with OS ? if yes , you need related lib , for example , MQX, please build "...\KSDK_1.0.0-KL43Z\usb\usb_core\device\build\kds\usbd_sdk_frdmkl43z48m_mqx".
Hope it helps
Alice
Sorry Alice for my bad english :smileysad:
I want to build virtual com bare metal project.
Once in a blank workspace:
- Import driver library and build, it works.
- Import usbd_sdk_frdmkl43z48m_bm, as you told me :smileyhappy:, and build, it works
- Import the dev_cdc_virtual_com_frdmkl43z48m_bm, it builds
I can plug the board to the PC and communicate with no problem. So it seems to work perfectly.
But when I want to write my own code inside I realize that it is not working in bare metal, OS_ADAPTER_SDK is selected, and if I change the adapter_cfg.h file to bare metal it stops working.
If I should put pictures of any message or something please tell me.
Regards,
Miguel
Hi Miguel,
Yes, I think is that : now on the KSDK_1.0.0-KL43Z, we only can use "OS_ADAPTER_SDK" .
the "OS_ADAPTER_MQX" and "OS_ADAPTER_BM" can not use now.
Because we can not checked out "adapter_bm.h" and "adapter_mqx.h" file under the USB file .
Hope it helps
ALice