Hello,
I have a FRDM-KL02Z and do some modified to it, then it can debug and KL02 MCU on my designed PCB. I also have a FRDM-KL05Z and a FRDM-KL25 board with same modified. I want to use these two FRDM board to debug and program KL02 MCU , but it is fail. the CW V10.4 shows can not find target MCU. image as following.
Do you think it possible to use FRDM-KL05Z and a FRDM-KL25 board to debug and program KL02 MCU?
Is there a simple ISP tool and engineering software to program KL02 MCU?
Thanks.
Kaka.
please refer answer as below: https://community.freescale.com/message/325654#325654
Hello Jun,
Thanks for your reply.
As my mentioned , i can use FRDM-KL02Z SWD port J1 to debug and program MKL02Z8VFG4 on my designed board. The FRDM-KL02Z board is cut wire same as https://community.freescale.com/message/325654#325654 said. but i only have one FRDM-KL02Z board. and i have one FRDM-KL05Z and one FRDM-KL25z board too. so i modified it accordingly ,not same way ,but same solution. These 2 FRDM boards can not used for KL02 MCU debug and program. I also read a note: http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/ , it said the author also can not make the FRDM-KL25z to program FRDM-KL05Z successful. Even that, i want to double check: Do you think it possible to use FRDM-KL05Z and a FRDM-KL25 board to debug and program KL02 MCU?
Is there a simple ISP tool and engineering software to program KL02 MCU?
Kaka
Hi Kaka,
I have no KL02, so I cannot say for sure if this works.
You can use the P&E OpenSDA MSD programmer to *program* another board (need the correct MSD), but not to debug.
If you need debug, you need a different OpenSDA firmware (USBDM, Segger or CodeRed).
See
- Debug External Processors with USBDM and Freedom Board | MCU on Eclipse
- Debugging FRDM-KL05Z with USBDM | MCU on Eclipse
- USBDM 4.10.5 supports now MCU10.4 | MCU on Eclipse
- Red Suite 5: Eclipse Juno, Processor Expert and unlimited FRDM-KL25Z | MCU on Eclipse
- Freedom Board with Segger OpenSDA Debug Firmware | MCU on Eclipse
Hope this helps