How to get MK51DX128CLH7 into MCUXpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get MK51DX128CLH7 into MCUXpresso?

Jump to solution
1,258 Views
Bert2
Contributor II

Hi,

I'm trying to find out how to work with the MK51DX128CLH7 in Xpresso. I found the MK51DX256CLK10 in a SDK but not the 128.

Do I have to use the generic M4?

Thanks in advance,

regards,

Bert

0 Kudos
1 Solution
1,244 Views
ErichStyger
Senior Contributor V

Just an idea: KDS (Kinetis Design Studio) with Processor Expert supports that device:

ErichStyger_0-1647593299440.png

 

What I did for similar cases:

a) using the possibility to install Processor Expert in to MCUXpresso IDE (did that for earlier versions, have not checked if this is still possible with 11.5). see https://mcuoneclipse.com/2017/04/09/mcuxpresso-ide-installing-processor-expert-into-eclipse-neon/ how this would look like. Otherwise: I used KDS to generate everything and then used MCUXpresso (see b))

b) import/port the KDS project with Processor Expert. https://mcuoneclipse.com/2018/07/27/porting-processor-expert-projects-to-mcuxpresso-ide/

I know this is a bit challenging, but worked for me for several projects with devices which are not supported by the NXP MCUXpresso SDK.

I hope this helps,

Erich

 

View solution in original post

4 Replies
1,254 Views
ErichStyger
Senior Contributor V

If they share the same peripherals, but are only different by the flash size, you should be able to use the smaller part, but change the linker file for the larger memory size.

0 Kudos
1,249 Views
Bert2
Contributor II

Hi, thanks for your quick answer. Unfortunately the devices differ in pinout (case) and peripherals.

0 Kudos
1,245 Views
ErichStyger
Senior Contributor V

Just an idea: KDS (Kinetis Design Studio) with Processor Expert supports that device:

ErichStyger_0-1647593299440.png

 

What I did for similar cases:

a) using the possibility to install Processor Expert in to MCUXpresso IDE (did that for earlier versions, have not checked if this is still possible with 11.5). see https://mcuoneclipse.com/2017/04/09/mcuxpresso-ide-installing-processor-expert-into-eclipse-neon/ how this would look like. Otherwise: I used KDS to generate everything and then used MCUXpresso (see b))

b) import/port the KDS project with Processor Expert. https://mcuoneclipse.com/2018/07/27/porting-processor-expert-projects-to-mcuxpresso-ide/

I know this is a bit challenging, but worked for me for several projects with devices which are not supported by the NXP MCUXpresso SDK.

I hope this helps,

Erich

 

1,238 Views
Bert2
Contributor II

Thank you Erich,

that will probably be my way. I did not look into the older IDE because the website did redirect me to the newer one...

Thanks very much!

0 Kudos