How does IEHOST in USBx_ADDINFO get cleared in the K20 USBOTG module?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does IEHOST in USBx_ADDINFO get cleared in the K20 USBOTG module?

510件の閲覧回数
wre
Contributor III

Hi.  After configuring the K20 USBOTG module to be a device the IEHOST bit is still set.  What is required to clear IEHOST?

Thanks.

ラベル(2)
タグ(4)
0 件の賞賛
2 返答(返信)

403件の閲覧回数
albertovargas
NXP Employee
NXP Employee

Hi Bill,

This register is used during the initialization of the module and it can't be changed on the fly.

If you need to change it on the fly, check USB On-The-Go or Duall Role configuration for it

0 件の賞賛

403件の閲覧回数
wre
Contributor III

Thanks for the reply.  I understand that it can not be cleared (to indicate Device) directly.  I'm trying to understand what I'm missing in my configuration of the USBOTG module that keeps IEHOST set.  In other words, after I configure the module I would expect IEHOST to be cleared but it isn't.  My assumption is that I'm missing something in the configuration but I don't know what. 

Bill

0 件の賞賛