Hi, pgo, will USBDM support the new KDS ide soon?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, pgo, will USBDM support the new KDS ide soon?

938 次查看
TOMXUE
Contributor II

Hi, pgo:

The new KDS ide is released recently. And will you prepare to support it for USBDM?

BTW, thanks for ypur genie work on USBDM.

Tao

From Tsinghua University

3 回复数

600 次查看
pgo
Senior Contributor V

Update on this is available:

Using USBDM with Kinetis Design Studio

600 次查看
pgo
Senior Contributor V

Hi Tao,

I have applied for the BETA download but it is not available at the moment. 

I will have a look when it is available.

PS> You could try USBDM+Eclipse+GNU Tools for an alternative  This works on Linux + Windows.

http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/code_sourcery_install_page.html

bye

600 次查看
perlam_i_au
Senior Contributor I

In this case you have to ask to USBDM developers, at this moment they have not mentioned nothing regard KDS support but as long as Kinetis devices use the same debugger interfaces (does not matter if you are using CodeWarrior or KDS) I hope USBDM will support KDS soon.

0 项奖励
回复