GoMCUxpresso conflict

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GoMCUxpresso conflict

跳至解决方案
1,044 次查看
pietrodicastri
Senior Contributor II

Good morning

I have a project imported from the KDS. Whe I try to build it gives this message

14:45:13 **** Clean-only build of configuration Debug2 for project Capas2p0_008 ****
make clean
MAKE Version 5.41 Copyright (c) 1987, 2014 Embarcadero Technologies, Inc.
Error makefile 6: Command syntax error
Error makefile 11: Command syntax error
Error makefile 12: Command syntax error
Error makefile 13: Command syntax error
Error makefile 14: Command syntax error
Error makefile 15: Command syntax error

 

and more of.
It seems it is conflicting with the Embarcadero make. 
What to do?

Thank You

Pietro

0 项奖励
回复
1 解答
959 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @pietrodicastri,

Could you please give us more details about what you are doing? Which MCUXpresso IDE version are you using? Which OS do you have both in VBox and your computer? From which microcontroller are you importing the project? Is the project an example code or your own development?

At the meantime, could you please take a look at the following information?

Kind regards, Raul.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
960 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @pietrodicastri,

Could you please give us more details about what you are doing? Which MCUXpresso IDE version are you using? Which OS do you have both in VBox and your computer? From which microcontroller are you importing the project? Is the project an example code or your own development?

At the meantime, could you please take a look at the following information?

Kind regards, Raul.

0 项奖励
回复
921 次查看
pietrodicastri
Senior Contributor II
I reinstalled the KDS and it is working..
Thank You
0 项奖励
回复
926 次查看
pietrodicastri
Senior Contributor II

Good morning

I am using Windows 10 x64, MCUXpresso v11.7.1_9221.

In the VBOX I use the same operating system. The project is using the K64, and it is a huge development not imported from any example. 
The project has worked for years on KDS. Possibly after the installation of the Embarcadero CBuilder new release the problem started. The KDS does not find the JTAG without any consistent message other than a generic error. The MCUxpresso does not want to build at all because is trying to use the make of Embarcadero.
I tried to test the MCUxpresso with an example project  and it works. 

That's all.
It seems something went wrong during the export. But I would prefer to use the KDS still.
Thank You

Pietro

0 项奖励
回复
1,042 次查看
pietrodicastri
Senior Contributor II
I specify the tool works with other projects. Something related to the importing is producing the error
0 项奖励
回复
981 次查看
pietrodicastri
Senior Contributor II
If I install on a VBox on the same PC it works.
Please suggest something. It is difficult to work on the VBox...
Thank You
0 项奖励
回复