I'm trying to communicate at 2.5Mbps using uart1 on mk10d.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm trying to communicate at 2.5Mbps using uart1 on mk10d.

1,323 Views
tj_P
Contributor I

I want to use uart1 and dma to communicate rs485 at a transmission rate of 2.5mbps.

 

 

After the data is sent, it takes approximately 30 us seconds for the response to start in slave.

At this time, the first byte fills up with 0x00 intermittently, so can you suggest a solution for this?

0 Kudos
Reply
1 Reply

1,277 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @tj_P 

Can you tell me the clock speed of you MK10? 120MHz, 100MHz, 75MHz or 50MHz.

Can you provide me more details please? What do you mean with " for the response to start in slave"? UART does not uses master/slave modes.

Best Regards, Miguel.

0 Kudos
Reply