GoMCUxpresso conflict

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GoMCUxpresso conflict

ソリューションへジャンプ
1,049件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I have a project imported from the KDS. Whe I try to build it gives this message

14:45:13 **** Clean-only build of configuration Debug2 for project Capas2p0_008 ****
make clean
MAKE Version 5.41 Copyright (c) 1987, 2014 Embarcadero Technologies, Inc.
Error makefile 6: Command syntax error
Error makefile 11: Command syntax error
Error makefile 12: Command syntax error
Error makefile 13: Command syntax error
Error makefile 14: Command syntax error
Error makefile 15: Command syntax error

 

and more of.
It seems it is conflicting with the Embarcadero make. 
What to do?

Thank You

Pietro

0 件の賞賛
返信
1 解決策
964件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @pietrodicastri,

Could you please give us more details about what you are doing? Which MCUXpresso IDE version are you using? Which OS do you have both in VBox and your computer? From which microcontroller are you importing the project? Is the project an example code or your own development?

At the meantime, could you please take a look at the following information?

Kind regards, Raul.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
965件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @pietrodicastri,

Could you please give us more details about what you are doing? Which MCUXpresso IDE version are you using? Which OS do you have both in VBox and your computer? From which microcontroller are you importing the project? Is the project an example code or your own development?

At the meantime, could you please take a look at the following information?

Kind regards, Raul.

0 件の賞賛
返信
926件の閲覧回数
pietrodicastri
Senior Contributor II
I reinstalled the KDS and it is working..
Thank You
0 件の賞賛
返信
931件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I am using Windows 10 x64, MCUXpresso v11.7.1_9221.

In the VBOX I use the same operating system. The project is using the K64, and it is a huge development not imported from any example. 
The project has worked for years on KDS. Possibly after the installation of the Embarcadero CBuilder new release the problem started. The KDS does not find the JTAG without any consistent message other than a generic error. The MCUxpresso does not want to build at all because is trying to use the make of Embarcadero.
I tried to test the MCUxpresso with an example project  and it works. 

That's all.
It seems something went wrong during the export. But I would prefer to use the KDS still.
Thank You

Pietro

0 件の賞賛
返信
1,047件の閲覧回数
pietrodicastri
Senior Contributor II
I specify the tool works with other projects. Something related to the importing is producing the error
0 件の賞賛
返信
986件の閲覧回数
pietrodicastri
Senior Contributor II
If I install on a VBox on the same PC it works.
Please suggest something. It is difficult to work on the VBox...
Thank You
0 件の賞賛
返信