GPIO at 1.4V - KEA-128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO at 1.4V - KEA-128

508 次查看
vigneshbalaji
Senior Contributor I

Hi,

    I am running 2 KEA128's at 3.2 V by giving VDD externally so that all the GPIO's are at 3.2v. I am using the dev boards(TRK-KEA128 boards).

From Board 1, I give input to Board 2. I make the input to board 2 from board 1 as high and low. I see that after making inputs high and low to board 2 for sometime, The voltage on board1 and board2 becomes 1.5 V while it is supposed to be zero on the corresponding pins. But if i remove the connection between the pins both pins on board 1 and board 2 are zero but if i connect it back they go to 1.5 V. Can anyone explain me the reason for this?

0 项奖励
回复
1 回复

405 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

    This question is the same question as your another post:

KEA128 GPIO at 1.4V 

  Please check my answer in that post.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复