Hello,
I think I already know the answer, but maybe I can get a happy surprise if I ask here.
I have a FRDM-KL43Z board which was working perfectly until now.
Now, when I plug it into the USB (K20 openSDA and the direct KL43 USB connector as well) the KL43 IC gets very hot, very fast. The board, K20 openSDA interface is recognized and mounted correctly, however I am unable to upload any code to KL43, the screen below keep showing:
I was going to probe the board to check voltages and components, but it gets hot very fast so I cant keep it on for longer than a few seconds.
The last sketch I uploaded was a simple "HELLO WORLD" LPUART test (send it every second) using OSA/FREERTOS.
Simple questions:
Is it bricked :smileycry: ?
If not, what can I do to resurect it :smileyhappy: ?
if yes, do you think I can still use the openSDA interface as debugger for other boards ??
Thanks.
解決済! 解決策の投稿を見る。
Hi, Thiago,
I think the KL43 chip on FRDM-KL43 has broken down for unknown reason, you have to change another chip. You can order another FRDM-KL43 or request a KL43 sample from Freescale website and solder it yourself on the damaged board.
BR
XiangJun Rong
Hi, Thiago,
I think the KL43 chip on FRDM-KL43 has broken down for unknown reason, you have to change another chip. You can order another FRDM-KL43 or request a KL43 sample from Freescale website and solder it yourself on the damaged board.
BR
XiangJun Rong
Yeah, I think that I will try your suggestion.
I have already removed the MKL43 and now I will test the whole board before soldering a new one.... Hopefully it will come back to life !
EDIT
Yeah, as expected, replaced the MCU and now it works again.... thanks !