FRDM-KL25Z not giving 3v3 and also gets over heated on regulator side

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL25Z not giving 3v3 and also gets over heated on regulator side

476件の閲覧回数
krishnakumargan
Contributor I

Dear Freescale engineers,

  In FRDM - KL25Z, Am driving Vin(input voltage) as 5volt. I am not able

to get 3.3v with reference to ground, instead of 3.3v am getting

2.2volt in 3v3 pinout, and also Voltage regulator and microcontroller

getting more hotter.

Thanks & Regards,

krishnakumar.G

Hetrogenous Communications Technologies Pvt Ltd.

No.25, Block - 2, 2 nd floor, SIDCO Indusrtrial Estate, Guindy,

Chennai - 600032.

cell : +91 - 9965899278

email : krishnakumar@hetrogenous.com

0 件の賞賛
1 返信

357件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Krishnakumar,

Obviously, there's some errors with the board, then cause the voltage level drop.

And I'd like to confirm with you whether the board works in standalone mode or not when you measure the 3v3 voltage of the FRDM-KL25.

I've also checked my board on hand, it can supply 3.3v for MCU.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛