FRDM-KL25Z issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KL25Z issue

818 次查看
andy_yang
Contributor I

Hi,

When I update frdm-kl25z, first press reset button and plug usb can find boot loader disk, then copy MSD-FRDM-KL25Z_Pemicro_v105.SDA into bootloader disk, unplug usb, then plug usb can't connect bootloader at all. please help this.

标签 (1)
0 项奖励
回复
3 回复数

635 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

After customer Copy & paste or drag & drop the MSD Flash Programmer Application (MSD-FRDM-KL25Z_Pemicro_v105.SDA)to the BOOTLOADER drive. Then plug USB port (SDA) again, if customer could find below [FRDM-KL25Z] disk display at computer panel?

pastedImage_1.png

pastedImage_2.png

What's your FRDM-KL25Z board hardware version?

My FRDM-KL25Z board hardware version is below:

pastedImage_3.png
Thank you for the attention.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

635 次查看
andy_yang
Contributor I

Hi Hui Ma,

Yes, it is same version with your board version 700-27556 Rev A1 and Sch-27556 Rev F.

Now we can get 6 files after copy MSD-FRDM-KL25Z_Pemicro_v105.SDA this file into bootloader disk, after this we copy blinky_blue.srec into disk, then unplug USB, again plug usb to PC, but only see board LED D4 light green, D3 not light blue, that is the problem, we are not sure if the board already damaged or not? Please help clarify this or if can repair it.

Best Regards

Andy Yang (Test Engineering Team)

Cell: +86 13760770188<tel:%2B86%20186%202090%201454>

Desk: +86 (020) 2805 5079<tel:%2B86%20%28020%29%202911%203200>

No. 1199, Hulin Road, Huangpu District, Guangzhou, Guangdong (510700), China

0 项奖励
回复

635 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I don't find your mentioned issue on my site. The D3 was blinked with blue light (blinky_blue.srec).

Could you using scope to check if the KL25's PTD1 pin with period GPIO toggle signals?

You also could probe at TP17 (test point).

pastedImage_1.png


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复