Hi All,
I am using FRDM-KEAZ128Q80 board for my application and i need to communicate with CAN bus.
i got MSCAN driver code for KEA128 and i am using
TEST_CASE_FUNC(Demo_Transmit_DataFrame);//set different parameter to choose other test case to run
also its working fine and i am able to receive the data through CAN bus in another controller but problem is when i am calling TEST_CASE_FUNC(Demo_Transmit_DataFrame); for every 1 sec its going to sleep mode and it is working only time after that MSCAN is going into sleep mode so please anybody can help me out how to send data continuously without going into sleep mode.
i attached my main file and MSCAN driver please find the attachment.
Thanks
Shoaib Ahmed
Original Attachment has been moved to: main.c.zip
Original Attachment has been moved to: MSCAN_Driver+FRDM_KEA128-Example.zip
I am working on FRDM-KEAZ128_MSCAN example on board FRDM-keaz128 board. Both transmit and receive codes are working. I want to make the interrupt based receive function that means receive function should be call when interrupt occur. Currently, it is calling in the main file.
I looked over my board and J107 is in about the center of the board and needs a jumper across pins 2 and 3 to work correctly so I am a little confused by the suggested pins to use for the CAN example? Any help with figuring out what pins to use with this example would be greatly appreciated!