I am not new to microcontrollers, but very new to mbed controllers - new as in, blinky_led sample code bricked my controller 10 minutes after plugging it in for the first time.
For a few minutes, after loading blinky_led and trying to move to the next example, I was stuck with the controller mounting and showing up as bootloader. It would periodically reboot and remount every minute or so. So I tried updating the firmware by dragging-and-dropping the .bin file from FRDM-K66F | Mbed . Now the board doesn't even light up when plugged into USB and Windows doesn't recognize any device being plugged in. If I plug into the power port, blinky_led will run.
I have a second board but I'm afraid to use it. I plugged it in hoping that I could use it to install the Windows ARM serial driver, as I was receiving "no microcontroller found" with the bricked one - nope still get error despite this being the very first instruction on the aforementioned mbed website. So I tried to do this right, and held down reset to go into bootloader mode, and at the beginning of a remounting cycle, tried to copy over the firmware. NOPE! firmware is 95kB and I only have 92kB of freespace on the board! Also, the article says DAPLink needs to be upgraded if it mounts as "bootloader" - ok, but of course, there is no FRDM-K66F listed in the table: DAPLink bootloader update | Mbed . I would use the K64F, but its such a fragile piece of equipment, that I'm afraid to.
None of the instructions to keep this delicate thing from dying seem to work. My second board is now stuck in bootloader mode, probably soon to be bricked as well. Please help. I want to use this board, but I'm frustrated by how out-of-the-box instructions don't work and can actually kill the board. I haven't even tried anything unique yet.
EDIT:
Got board #2 working ok. For some reason I showed 98kB of free space when loaded into Linux and could copy the firmware, which made the device appear as a drive called FRDM-K66FD. And then the serial driver would install correctly. I'm still stuck short of having a probe to allow debugging. I checked my downloads, I believe I dropped blinkyled.bin onto the BootLoader drive which killed the first board - I did not drop firmware. Hopefully there is a repair for this mistake.
Have you already updated the bootloader itself to a version working with your machine? See https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/
Hi E F,
Please refer the answer in Really Hard Bricked FRDM-K22F Boards.
In any case, you need a separate/external device to re-program the bootloader.
there is no FRDM-K66F listed in the table
You can download the latest bootloader and firmware application of DAPLink rev0244. I have also attached these two files here.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------