Ethernet for K60N512VMD100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet for K60N512VMD100

1,185 Views
karthikas
Contributor IV

I am working with tower kit (TWR-K60N512) , Can anyone send me Ethernet stack for the mentioned board to start working on this board .

I am using keil 4 platform. 

Labels (1)
Tags (2)
0 Kudos
6 Replies

833 Views
ivadorazinova
NXP Employee
NXP Employee

Hello,

please what is your MCU?

For TWR-K60N512 you could find useful:

In latest FNET version is support for IAR and KDS, so is needed to add FNET to it by yourself.

  • RTCS stack under MQX - examples for your board as Ethernet to Serial, GPRS connection application, HTTP server application, Iperf, Shell and Snmp

Please see attached file.

I hope this helps you.

Have a great day.

Iva

0 Kudos

833 Views
karthikas
Contributor IV

MCU is MK60N512VMD100

Still I don't have clarity on how to get stack . Can you attach the stack which are compatible with KEIL 4

0 Kudos

833 Views
ivadorazinova
NXP Employee
NXP Employee

RTCS stack is fully compatible with TWR-K60N512 and Keil 4.

It is needed to go on MQX™ Classic Software Solutions|NXP and download MQX RTOS 4.2.0.exe

Please,see the document above for more details.

fNET is tested with Keil 5.11

Best Regards,

Iva

0 Kudos

833 Views
karthikas
Contributor IV

  Hello .,

I have downloaded MQX RTOS 4.2.0.exe ​ and tried to open with Keil 4 , but its not getting opened.

Path of file I am using : C:\Freescale\Freescale_MQX_4_2\rtcs\build\uv4\rtcs_twrk60n512.

It was showing :: The project file has a newer major version number which is not compatible with this programmer version.

Tell me whether I have to open with Keil 5 or other version ,

0 Kudos

833 Views
ivadorazinova
NXP Employee
NXP Employee

Hi KARTHIK A S ,

Freescale MQX RTOS was compiled and tested with these

development tools:

    • Kinetis Development Studio version 3.0.0

    • Support available for Kinetis devices

    • See build projects in the Kinetis Design Studio subdirectory

    • Makefile build option: TOOL=kds

• CodeWarrior Development Studio for Microcontrollers

version 10.6

    • Support available for Kinetis and ColdFire devices

    • See build projects in the cw10gcc subdirectory

    • Makefile build option (Kinetis GCC only): TOOL=cw10gcc

• IAR Embedded Workbench for ARM® Version 7.40.1

    • Support available for Kinetis and Vybrid devices

    • See build projects in iar subdirectories

    • Makefile build option: TOOL=iar

• ARM Development Studio 5 (DS-5™) version 5.20.1

• DS-5 Starter Kit for Vybrid Controllers version 5.20.1

• DS-5 Vybrid Controller Edition 5.20.1

    • Support available for Vybrid devices

    • See build projects in the ds5 subdirectory

    • Makefile build option: TOOL=ds5

• ARM-MDK - Keil® μVision® version 5.14.0 and

• ARM-MDK Legacy Pack add-in - extending MDK with MQX RTOS Task Aware Debugger plugin

    • Support available for Kinetis devices

    • See build projects in the uv4 subdirectories

    • Makefile build option: TOOL=uv4

• GNU Tools for ARM Embedded Processors revision 4.8-2014-q3-update

    • Support available for Kinetis and Vybrid devices

    • Makefile build option: TOOL=gcc_arm

• Makefile support (mingw32-make version 4.8.4)

    • Library makefiles are located in <MQX_root_dir>/build/make/<board>

    • Application makefiles are located in <example_dir>/make/<board>

Best Regards,

Iva

0 Kudos

833 Views
Masmiseim
Senior Contributor I
0 Kudos