Driver stepper motor ,KEA or KV?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driver stepper motor ,KEA or KV?

940件の閲覧回数
kigerzhang
Contributor III

Now there is a  medical automatic  injector instrument  project need  a MCU to control a stepper motor .

The MC34932 is planed to be  as the driver .

The KVxx is dedicated for motor driver . But the KEA xx seems more reliable.

The KEA series   and  KVxx  series  which is the best choice?

0 件の賞賛
返信
1 返信

601件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

It is really depend on your application, the requirement of your stepper motor.

Kinetis V Series MCUs are based upon the ARM® Cortex®-M0+, Cortex-M4 and Cortex-M7 cores and are designed for a wide range of BLDC, PMSM and ACIM motor control and digital power conversion applications.

The Kinetis EA series is an entry point to the broad ARM ecosystem and features:

  • A low-power ARM Cortex-M0+ core and 8–128 KB of embedded flash
  • Excellent EMC/ESD, high temperature and low radiated emissions
  • Scalable, highly robust performance solution for cost-sensitive automotive applications.

Attached you will find a PPT on this topic maybe helpful to you.

0 件の賞賛
返信