Do Kinetis K22 has internal pullups on the SDHC peripheral lines?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do Kinetis K22 has internal pullups on the SDHC peripheral lines?

739件の閲覧回数
pasqualelongo
Contributor I

Or i need to put them external?
Thanks,

Pasquale

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

570件の閲覧回数
pasqualelongo
Contributor I

Thanks Mark and Paul,

I'll perform some tests using internal pullups, if i'll found problems i'll install external.

Will keep you updated

Pasquale

0 件の賞賛
返信

570件の閲覧回数
mjbcswitzerland
Specialist V

Pasquale

You can decide whether pull-ups are enabled or not when configuring each pin. See PORTn_PCRx register.

The pull-up resistors will have a wider tolerance spread than external ones though.

Regards

Mark

0 件の賞賛
返信

570件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Longo

I agree with Mark. It is better to add external pull-up resistor. The internal resistor is a weak pull-up. So you need add a strong pull-up external to ensure communication is good on no good layout condition. Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信