Hi
You define which peripheral trigger is used for each DMA channel in the DMAMUX.
Registers are
DMAMUX0_CHCFG0
DMAMUX0_CHCFG1
DMAMUX0_CHCFG2
DMAMUX0_CHCFG3
Regards
Mark
hi Mark,
Thank you for help.
I find your said , use DMAUX0_CHCFGN -> SOURCE define , while where can find the peripheral trigger's slot number? for example , now i use UART _DMA trigger DMA0 , the slot number is ? or the DMAMUX0_CHCFG0 is ?
Best Regards
Linda
Linda
These are the trigger defines that I use when working with the KL devices (not all triggers are available on particular devices)
Regards
Mark
#define DMAMUX_CHCFG_SOURCE_DISABLED | 0 | // 0x00 | |
#define DMAMUX_CHCFG_SOURCE_UART0_RX | 2 | // 0x02 UART0 RX - DMAMUX_CHCFG_xx are available on DMA MUX 0 and on DMA MUX 1 (when available) | |
#define DMAMUX_CHCFG_SOURCE_UART0_TX | 3 | // 0x03 UART0 TX | |
#define DMAMUX_CHCFG_SOURCE_UART1_RX | 4 | // 0x04 UART1 RX | |
#define DMAMUX_CHCFG_SOURCE_UART1_TX | 5 | // 0x05 UART1 TX | |
#define DMAMUX_CHCFG_SOURCE_UART2_RX | 6 | // 0x06 UART2 RX | |
#define DMAMUX_CHCFG_SOURCE_UART2_TX | 7 | // 0x07 UART2 TX | |
#define DMAMUX_CHCFG_SOURCE_UART3_RX | 8 | // 0x08 UART3 RX | |
#define DMAMUX_CHCFG_SOURCE_UART3_TX | 9 | // 0x09 UART3 TX | |
#define DMAMUX_CHCFG_SOURCE_UART4_RX | 10 | // 0x0a UART4 RX | |
#define DMAMUX_CHCFG_SOURCE_UART4_TX | 11 | // 0x0b UART4 TX | |
#define DMAMUX_CHCFG_SOURCE_UART5_RX | 12 | // 0x0c UART5 RX | |
#define DMAMUX_CHCFG_SOURCE_UART5_TX | 13 | // 0x0d UART5 TX | |
#define DMAMUX_CHCFG_SOURCE_I2S0_RX | 14 | // 0x0e I2S0 RX | |
#define DMAMUX_CHCFG_SOURCE_I2S0_TX | 15 | // 0x0f I2S0 TX | |
#define DMAMUX_CHCFG_SOURCE_SPI0_RX | 16 | // 0x10 SPI0 RX | |
#define DMAMUX_CHCFG_SOURCE_SPI0_TX | 17 | // 0x11 SPI0 TX | |
#define DMAMUX_CHCFG_SOURCE_SPI1_RX | 18 | // 0x12 SPI1 RX | |
#define DMAMUX_CHCFG_SOURCE_SPI1_TX | 19 | // 0x13 SPI1 TX | |
#define DMAMUX_CHCFG_SOURCE_SPI2_RX | 20 | // 0x14 SPI2 RX | |
#define DMAMUX_CHCFG_SOURCE_SPI2_TX | 21 | // 0x15 SPI2 TX | |
#define DMAMUX0_CHCFG_SOURCE_I2C0 | 22 | // 0x16 I2C0 - DMAMUX0_CHCFG_xx are only available on DMA MUX 0 | |
#define DMAMUX0_CHCFG_SOURCE_I2C1_2 | 23 | // 0x17 I2C1 (or I2C2) | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C0 | 24 | // 0x18 FTM0/TPM0 channel 0 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C1 | 25 | // 0x19 FTM0/TPM0 channel 1 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C2 | 26 | // 0x1a FTM0/TPM0 channel 2 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C3 | 27 | // 0x1b FTM0/TPM0 channel 3 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C4 | 28 | // 0x1c FTM0/TPM0 channel 4 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C5 | 29 | // 0x1d FTM0/TPM0 channel 5 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C6 | 30 | // 0x1e FTM0/TPM0 channel 6 | |
#define DMAMUX_CHCFG_SOURCE_FTM0_C7 | 31 | // 0x1f FTM0/TPM0 channel 7 | |
#define DMAMUX0_CHCFG_SOURCE_FTM1_C0 | 32 | // 0x20 FTM1/TPM1 channel 0 | |
#define DMAMUX0_CHCFG_SOURCE_FTM1_C1 | 33 | // 0x21 FTM1/TPM1 channel 1 | |
#define DMAMUX0_CHCFG_SOURCE_FTM2_C0 | 34 | // 0x22 FTM2/TPM2 channel 0 | |
#define DMAMUX0_CHCFG_SOURCE_FTM2_C1 | 35 | // 0x23 FTM2/TPM2 channel 1 | |
#define DMAMUX_CHCFG_SOURCE_IEEE1588_T0 | 36 | // 0x24 IEEE 1588 timer 0 (alternative) | |
#define DMAMUX0_CHCFG_SOURCE_FTM3_C1 | 36 | // 0x24 FTM3 channel 1 | |
#define DMAMUX_CHCFG_SOURCE_IEEE1588_T1 | 37 | // 0x25 IEEE 1588 timer 1 (alternative) | |
#define DMAMUX0_CHCFG_SOURCE_FTM3_C2 | 37 | // 0x25 FTM3 channel 2 | |
#define DMAMUX_CHCFG_SOURCE_IEEE1588_T2 | 38 | // 0x26 IEEE 1588 timer 2 (alternative) | |
#define DMAMUX0_CHCFG_SOURCE_FTM3_C3 | 38 | // 0x26 FTM3 channel 3 | |
#define DMAMUX_CHCFG_SOURCE_IEEE1588_T3 | 39 | // 0x27 IEEE 1588 timer 3 (alternative) | |
#define DMAMUX_CHCFG_SOURCE_ADC0 | 40 | // 0x28 ADC0 | |
#define DMAMUX_CHCFG_SOURCE_ADC1 | 41 | // 0x29 ADC1 | |
#define DMAMUX0_CHCFG_SOURCE_CMP0 | 42 | // 0x2a CMP0 | |
#define DMAMUX0_CHCFG_SOURCE_CMP1 | 43 | // 0x2b CMP1 | |
#define DMAMUX0_CHCFG_SOURCE_CMP2 | 44 | // 0x2c CMP2 | |
#define DMAMUX_CHCFG_SOURCE_DAC0 | 45 | // 0x2d DAC0 | |
#define DMAMUX_CHCFG_SOURCE_DAC1 | 46 | // 0x2e DAC1 | |
#define DMAMUX0_CHCFG_SOURCE_CMT | 47 | // 0x2f CMT | |
#define DMAMUX0_CHCFG_SOURCE_PDB | 48 | // 0x30 PDB | |
#define DMAMUX0_CHCFG_SOURCE_PORTA | 49 | // 0x31 port A | |
#define DMAMUX0_CHCFG_SOURCE_PORTB | 50 | // 0x32 port B | |
#define DMAMUX0_CHCFG_SOURCE_PORTC | 51 | // 0x33 port C | |
#define DMAMUX0_CHCFG_SOURCE_PORTD | 52 | // 0x34 port D | |
#define DMAMUX0_CHCFG_SOURCE_PORTE | 53 | // 0x35 port E | |
#define DMAMUX0_CHCFG_SOURCE_TPM0_OVERFLOW | 54 | // 0x36 TPM0 overflow | |
#define DMAMUX0_CHCFG_SOURCE_TPM1_OVERFLOW | 55 | // 0x37 TPM1 overflow | |
#define DMAMUX0_CHCFG_SOURCE_TPM2_OVERFLOW | 56 | // 0x38 TPM2 overflow | |
#define DMAMUX0_CHCFG_SOURCE_TSI | 57 | // 0x39 TSI | |
#define DMAMUX_CHCFG_TRIG | 0x40 | // DMA channel trigger enable | |
#define DMAMUX_CHCFG_ENBL | 0x80 | // DMA channel enable |
Hi Mark,
Thank for your help.
And i have another question, now I want use DMA transmit ADC result data. I need collect two different signals use two ADC channles . And the in kl25 , all of the adc channels dma trigger are called ADC0, my question is now I can't use two DMA channals transmit two ADC data , do you have any good idea ?
Thank you !
Linda
Linda
The KL25 has one ADC controller. You can configure it for HW triggered mode so that it samples two channels automatically.
The results are available in ADC0_RA and ADC0_RB so it is possible to transfer these by configuring a DMA channel to copy two 16 bit words from ADC0_RA address on each trigger. The result is the two channels at the destination - if a buffer, the two channels will be stored Channel A, Channel B, Channel A, Channel B etc,
Or you can program two DMA channels with the same trigger and each one can copy either ADC0_RA or ADC0_RB to a buffer so that the channel data is not alternating.
Regards
Mark