Hi all,
I have a TWR-K20D72M board without an 8MHz crystal, is it possible to start MQX without?
I tried to modify the _bsp_initialize_hardware() function to exclude initialisation of the oscillator and MQX boots but the _time_delay(x) calls never return.
Has anyone run MQX without the 8MHz oscillator and could you point me to the right direction to get the board running in FLL Engaged Internal (FEI) clock mode or FLL Bypassed Internal (FBI) clock mode (I believe these two modes do not depend on the oscillator).
Best regards,
Christos
解決済! 解決策の投稿を見る。
Hello christos,
If you want to change the clock settings of any BSP of MQX, you could refer to the document named “How-to Change Default Clock Settings in Kinetis BSPs”, available at the following path:
C:\Freescale\Freescale_MQX_4_0\doc\tools\cw\
I have attached to this post the mentioned document. Hope this will be useful for you.
Best regards!
/Carlos
Christos
I had the same problem with the TWR-K20D50M. The solution was to go to the toolbar lightning bolt item, select Import Flash Task, then select the correct processor from the list. Apparently the chip was not getting flashed properly, evidenced by an error related to address 0xfffffffe.
Hello christos,
If you want to change the clock settings of any BSP of MQX, you could refer to the document named “How-to Change Default Clock Settings in Kinetis BSPs”, available at the following path:
C:\Freescale\Freescale_MQX_4_0\doc\tools\cw\
I have attached to this post the mentioned document. Hope this will be useful for you.
Best regards!
/Carlos