vision4legacy2_1_13PE_ISR.zip is attached in my documents which should be visible.
When trying to utilize the ADC I get the PE ISR shown below. Previously using the DAC LDD caused this by not
using auto initialization in the component properties, but that didn't solve the ADC problem. Any help why this is happening?
PE_ISR(Cpu_Interrupt)
{
/* This code can be changed using the CPU component property "Build Options / Unhandled int code" */
PE_DEBUGHALT();
已解决! 转到解答。
I don't use PE, but why do you think it is the ADC?
I am thinking it is an "unhandled interrupt" but that does not mean it is a hard fault.
Does the passed in value, Cpu_Interrupt tell which interrupt it is?
I have no clue where I set use advanced editor :smileyhappy: the code which includes concole, timer, dac,etc
were all working perfectly. when trying to add high level bean I could only get one channel to convert. then the TIC gave me example using LDD which worked in their example but cause PE ISR in mine. I had the same issue getting PE ISR with DAC LDD before I set auto initialize in component setting. that didn't help for ADC.
What is a TIC?
If you click reply, then look in the upper right corner you will see a link that says "Use advanced editor".
That is one of the draw backs of using PE, it can be hard to integrate "other" code.
I would think the issue is that the sample code has a function ADC0_IRQHandler(), but since the PE interrupt table is different, it does not over ride the weak function defined in kinetis_sysinit.c in a non PE project. Does the sample code have such a function?
how can I upload the zip problem along side my questions and if you were to add an attachment, where would it show up? even my local Freescale FAE didn't know. I can email you the zip directly if you give me an address.
I don't know how to attach a file here. I uploaded it in my files. the tool bar just above this image does not show upload file. only text input, upload image, insert video, insert link, etc.